AnsweredAssumed Answered

Generate softaware interrupt..

Question asked by arbitrer on Jun 8, 2015
Latest reply on Jun 8, 2015 by peacock.jack.003
Hi,

I want to generate a software interrupt,.. ie;when I execute one step it should go to ISR and do some activities..

My scenario..
I'm using RTOS for my application. I am reading data from a FIFO and storing it to a buffer via DMA, so while the DMA is ongoing I want so send some packets via WIFI, but the thing is that for context switching it takes max 1ms which is too much, so if I do the conetxt switch with in ISR it'll be switched in 10microsec... this is why I need to generate a software interrupt

Please help me....

Outcomes