AnsweredAssumed Answered

Saving images from CMOS sensor on SD card

Question asked by Matt on Jun 7, 2015
Latest reply on May 8, 2017 by Clive One
Hi

I'm looking for a way to transfer 5MP images from OmniVision OV5640 camera sensor to SD card. OV5640 have 8-bit parallel interface. It also features compression engine so the output could be in JPEG format. Is the transfer possible with any of the STM32 microcontrollers? Shall I look at the models equipped with DCMI interface? Maybe if transfer would happend through DMA bus every STM32 model would be suitable to handle the transfer of JPEG images through GPIO ports?

Matt

Outcomes