AnsweredAssumed Answered

stm32 UART-DMA one character transfer problem

Question asked by mikhaylin.dmitry on Jun 1, 2015
Latest reply on Jun 2, 2015 by mikhaylin.dmitry
Hello! I'm using STM32F407 processor. When I'm trying to send 1 byte via USART-DMA (for example 0x72) I get two bytes "72 72" in terminal.If I send two or more bytes everything is okay. If I send something from terminal I can't receive one byte, only two or more bytes can be received. Maybe someone can help to solve this problem. Thanks.

Outcomes