AnsweredAssumed Answered

stm3210E_EVAL: USB, SDcard, NAND Flash

Question asked by satour.abou on May 15, 2015
Latest reply on May 15, 2015 by Clive One
Hello, 
I use the stm3210e_eval board.
I copmpiled the STM3210E-EVAL_FW_V2.1.0 using the IDE Coocox. everything is Ok.

but I have a problem at the level of USB, SDcard and the NAND Flash.
In fact, the STM3210E_EVAL support two logical unit number: the SDcard and the NAND flash.
I want delete the NAND and keep only the SDcard.
So I change uint32_t Max_Lun = 1; to uint32_t Max_Lun = 0; in usb_prop.c
but Windows don't detect the usb connection anymore !

I don't understand what !! any helps please ?

feel free to ask me more questions if I wasn't clear in the description of my problem.

thanks

Outcomes