AnsweredAssumed Answered

STM32F303 SPI alternative use of the NSS pin problem

Question asked by bigden.gary on May 12, 2015
Latest reply on May 15, 2015 by J.M.001
When using SPI2 PB12 is the NSS pin. However, I want to use PB12 as an output and not have it set or reset by the NSS when using SPI2. I thought I had done that by this line of code: 

SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;

However, when I try to use PB12 something is pulling it hard low. Any suggestions?

Outcomes