AnsweredAssumed Answered

Does the HAL support MMC?

Question asked by 65693 on May 12, 2015
Latest reply on May 24, 2018 by Matthew Staben
So in `SD_PowerON` there is a comment at the bottom that says `/* else MMC Card */`. `hsd->CardType` is never set to `MULTIMEDIA_CARD` which is defined in `stm32f4xx_hal_sd.h`, and read in `HAL_SD_WideBusOperation_Config`.

I have generated a project in the Cube and changed the `Mode` of `SDIO` to `eMMC 4 bits wide`, but it doesn't seem any different to the SD version.

Here is the function for reference:-

/**
  * @brief  Enquires cards about their operating voltage and configures clock
  *         controls and stores SD information that will be needed in future
  *         in the SD handle.
  * @param  hsd: SD handle
  * @retval SD Card error state
  */
static HAL_SD_ErrorTypedef SD_PowerON(SD_HandleTypeDef *hsd)
{
  SDIO_CmdInitTypeDef sdio_cmdinitstructure;
  __IO HAL_SD_ErrorTypedef errorstate = SD_OK;
  uint32_t response = 0, count = 0, validvoltage = 0;
  uint32_t sdtype = SD_STD_CAPACITY;
   
  /* Power ON Sequence -------------------------------------------------------*/
  /* Disable SDIO Clock */
  __HAL_SD_SDIO_DISABLE();
   
  /* Set Power State to ON */
  SDIO_PowerState_ON(hsd->Instance);
   
  /* 1ms: required power up waiting time before starting the SD initialization
     sequence */
  HAL_Delay(1);
   
  /* Enable SDIO Clock */
  __HAL_SD_SDIO_ENABLE();
   
  /* CMD0: GO_IDLE_STATE -----------------------------------------------------*/
  /* No CMD response required */
  sdio_cmdinitstructure.Argument         = 0;
  sdio_cmdinitstructure.CmdIndex         = SD_CMD_GO_IDLE_STATE;
  sdio_cmdinitstructure.Response         = SDIO_RESPONSE_NO;
  sdio_cmdinitstructure.WaitForInterrupt = SDIO_WAIT_NO;
  sdio_cmdinitstructure.CPSM             = SDIO_CPSM_ENABLE;
  SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
   
  /* Check for error conditions */
  errorstate = SD_CmdError(hsd);
   
  if(errorstate != SD_OK)
  {
    /* CMD Response Timeout (wait for CMDSENT flag) */
    return errorstate;
  }
   
  /* CMD8: SEND_IF_COND ------------------------------------------------------*/
  /* Send CMD8 to verify SD card interface operating condition */
  /* Argument: - [31:12]: Reserved (shall be set to '0')
  - [11:8]: Supply Voltage (VHS) 0x1 (Range: 2.7-3.6 V)
  - [7:0]: Check Pattern (recommended 0xAA) */
  /* CMD Response: R7 */
  sdio_cmdinitstructure.Argument         = SD_CHECK_PATTERN;
  sdio_cmdinitstructure.CmdIndex         = SD_SDIO_SEND_IF_COND;
  sdio_cmdinitstructure.Response         = SDIO_RESPONSE_SHORT;
  SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
   
  /* Check for error conditions */
  errorstate = SD_CmdResp7Error(hsd);
   
  if (errorstate == SD_OK)
  {
    /* SD Card 2.0 */
    hsd->CardType = STD_CAPACITY_SD_CARD_V2_0;
    sdtype        = SD_HIGH_CAPACITY;
  }
   
  /* Send CMD55 */
  sdio_cmdinitstructure.Argument         = 0;
  sdio_cmdinitstructure.CmdIndex         = SD_CMD_APP_CMD;
  SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
   
  /* Check for error conditions */
  errorstate = SD_CmdResp1Error(hsd, SD_CMD_APP_CMD);
   
  /* If errorstate is Command Timeout, it is a MMC card */
  /* If errorstate is SD_OK it is a SD card: SD card 2.0 (voltage range mismatch)
     or SD card 1.x */
  if(errorstate == SD_OK)
  {
    /* SD CARD */
    /* Send ACMD41 SD_APP_OP_COND with Argument 0x80100000 */
    while((!validvoltage) && (count < SD_MAX_VOLT_TRIAL))
    {
       
      /* SEND CMD55 APP_CMD with RCA as 0 */
      sdio_cmdinitstructure.Argument         = 0;
      sdio_cmdinitstructure.CmdIndex         = SD_CMD_APP_CMD;
      sdio_cmdinitstructure.Response         = SDIO_RESPONSE_SHORT;
      sdio_cmdinitstructure.WaitForInterrupt = SDIO_WAIT_NO;
      sdio_cmdinitstructure.CPSM             = SDIO_CPSM_ENABLE;
      SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
       
      /* Check for error conditions */
      errorstate = SD_CmdResp1Error(hsd, SD_CMD_APP_CMD);
       
      if(errorstate != SD_OK)
      {
        return errorstate;
      }
       
      /* Send CMD41 */
      sdio_cmdinitstructure.Argument         = SD_VOLTAGE_WINDOW_SD | sdtype;
      sdio_cmdinitstructure.CmdIndex         = SD_CMD_SD_APP_OP_COND;
      sdio_cmdinitstructure.Response         = SDIO_RESPONSE_SHORT;
      sdio_cmdinitstructure.WaitForInterrupt = SDIO_WAIT_NO;
      sdio_cmdinitstructure.CPSM             = SDIO_CPSM_ENABLE;
      SDIO_SendCommand(hsd->Instance, &sdio_cmdinitstructure);
       
      /* Check for error conditions */
      errorstate = SD_CmdResp3Error(hsd);
       
      if(errorstate != SD_OK)
      {
        return errorstate;
      }
       
      /* Get command response */
      response = SDIO_GetResponse(SDIO_RESP1);
       
      /* Get operating voltage*/
      validvoltage = (((response >> 31) == 1) ? 1 : 0);
       
      count++;
    }
     
    if(count >= SD_MAX_VOLT_TRIAL)
    {
      errorstate = SD_INVALID_VOLTRANGE;
       
      return errorstate;
    }
     
    if((response & SD_HIGH_CAPACITY) == SD_HIGH_CAPACITY) /* (response &= SD_HIGH_CAPACITY) */
    {
      hsd->CardType = HIGH_CAPACITY_SD_CARD;
    }
     
  } /* else MMC Card */
   
  return errorstate;
}

Outcomes