AnsweredAssumed Answered

SDRAM STM32F429 FMC SDRAM DELAY

Question asked by doopler on May 10, 2015
Latest reply on Oct 26, 2015 by waclawek.jan
Hi,
i am using STM32F429 and AS4C4M16S-6TIN memory (http://www.alliancememory.com/pdf/dram/64m-as4c4m16s.pdf) . and i have following problm: When i write some value and I trying read data from memory there is a  small change :
adress       value
2002ffd8   de111206
d00003d4  de115206


and after some delay it's looks like that


adress      value
2002ffd8   de111206
d00003d4  fe117206


pins are connected to memory in the same way like in discovery board.


here is a configuration function which i found in some page. I change some settings for that memory and now i dont know what can be wrong.


#define RCC_SYNC() __DSB()
#define SYSCLK_FREQ_168MHz
static void sdramCommandWait()
{
    for(int i=0;i<0xffff;i++)
        if((FMC_Bank5_6->SDSR & FMC_SDSR_BUSY)==0) return;
}




void configureSdram()
{
    //Enable all gpios
    RCC->AHB1ENR |= /*RCC_AHB1ENR_GPIOAEN |*/ RCC_AHB1ENR_GPIOBEN |
                    RCC_AHB1ENR_GPIOCEN | RCC_AHB1ENR_GPIODEN |
                    RCC_AHB1ENR_GPIOEEN | RCC_AHB1ENR_GPIOFEN |
                    RCC_AHB1ENR_GPIOGEN /*| RCC_AHB1ENR_GPIOHEN*/;
    RCC_SYNC();




    //First, configure SDRAM GPIOs
    GPIOB->AFR[0]=0x0cc00000;
    GPIOC->AFR[0]=0x0000000c;
    GPIOD->AFR[0]=0x000000cc;
    GPIOD->AFR[1]=0xcc000ccc;
    GPIOE->AFR[0]=0xc00000cc;
    GPIOE->AFR[1]=0xcccccccc;
    GPIOF->AFR[0]=0x00cccccc;
    GPIOF->AFR[1]=0xccccc000;
    GPIOG->AFR[0]=0x00cc00cc;
    GPIOG->AFR[1]=0xc000000c;




    GPIOB->MODER=0x00002800;
    GPIOC->MODER=0x00000002;
    GPIOD->MODER=0xa02a000a;
    GPIOE->MODER=0xaaaa800a;
    GPIOF->MODER=0xaa800aaa;
    GPIOG->MODER=0x80020a0a;




    //GPIOA->OSPEEDR=0xaaaaaaaa; //Default to 50MHz speed for all GPIOs...
    GPIOB->OSPEEDR=0xaaaaaaaa | 0x00003c00; //...but 100MHz for the SDRAM pins
    GPIOC->OSPEEDR=0xaaaaaaaa | 0x00000003;
    GPIOD->OSPEEDR=0xaaaaaaaa | 0xf03f000f;
    GPIOE->OSPEEDR=0xaaaaaaaa | 0xffffc00f;
    GPIOF->OSPEEDR=0xaaaaaaaa | 0xffc00fff;
    GPIOG->OSPEEDR=0xaaaaaaaa | 0xc0030f0f;
    ///GPIOH->OSPEEDR=0xaaaaaaaa;




    //Since we'we un-configured PB3/PB4 from the default at boot TDO,NTRST,
    //finish the job and remove the default pull-up
    GPIOB->PUPDR=0;




    //Second, actually start the SDRAM controller
    RCC->AHB3ENR |= RCC_AHB3ENR_FMCEN;
    RCC_SYNC();




    //SDRAM is a IS42S16400J -7 speed grade, connected to bank 2 (0xd0000000)
    //Some bits in SDCR[1] are don't care, and the have to be set in SDCR[0],
    //they aren't just don't care, the controller will fail if they aren't at 0
    FMC_Bank5_6->SDCR[0]=FMC_SDCR1_SDCLK_1// SDRAM runs @ half CPU frequency
                       | FMC_SDCR1_RBURST // Enable read burst
                       | 0;               //  0 delay between reads after CAS
    FMC_Bank5_6->SDCR[1]=0                //  8 bit column address
                       | FMC_SDCR1_NR_0   // 12 bit row address
                       | FMC_SDCR1_MWID_0 // 16 bit data bus
                       | FMC_SDCR1_NB     //  4 banks
                       | FMC_SDCR1_CAS_1; //  2 cycle CAS latency (F<133MHz)




    #ifdef SYSCLK_FREQ_180MHz
    //One SDRAM clock cycle is 11.1ns
    //Some bits in SDTR[1] are don't care, and the have to be set in SDTR[0],
    //they aren't just don't care, the controller will fail if they aren't at 0
    FMC_Bank5_6->SDTR[0]=(6-1)<<12        // 6 cycle TRC  (66.6ns>63ns)
                       | (2-1)<<20;       // 2 cycle TRP  (22.2ns>15ns)
    FMC_Bank5_6->SDTR[1]=(2-1)<<0         // 2 cycle TMRD
                       | (7-1)<<4         // 7 cycle TXSR (77.7ns>70ns)
                       | (4-1)<<8         // 4 cycle TRAS (44.4ns>42ns)
                       | (2-1)<<16        // 2 cycle TWR
                       | (2-1)<<24;       // 2 cycle TRCD (22.2ns>15ns)
    #elif defined(SYSCLK_FREQ_168MHz)
    //One SDRAM clock cycle is 11.9ns
    //Some bits in SDTR[1] are don't care, and the have to be set in SDTR[0],
    //they aren't just don't care, the controller will fail if they aren't at 0
    FMC_Bank5_6->SDTR[0]=(6-1)<<12        // 6 cycle TRC  (71.4ns>63ns) #63ns
                       | (2-1)<<20;       // 2 cycle TRP  (23.8ns>15ns) #21ns
    FMC_Bank5_6->SDTR[1]=(2-1)<<0         // 2 cycle TMRD #2
                       | (6-1)<<4         // 6 cycle TXSR (71.4ns>70ns) #63+1.5ns
                       | (5-1)<<8         // 4 cycle TRAS (47.6ns>42ns) #49ns
                       | (2-1)<<16        // 2 cycle TWR #2
                       | (2-1)<<24;       // 2 cycle TRCD (23.8ns>15ns)#21ns
    #else
    #error No SDRAM timings for this clock
    #endif




    FMC_Bank5_6->SDCMR=  FMC_SDCMR_CTB2   // Enable bank 2
                       | 1;               // MODE=001 clock enabled
    sdramCommandWait();




    //ST and SDRAM datasheet agree a 100us delay is required here.
    // In my memory is 200us
    delayUs(200);




    FMC_Bank5_6->SDCMR=  FMC_SDCMR_CTB2   // Enable bank 2
                       | 2;               // MODE=010 precharge all command
    sdramCommandWait();




    FMC_Bank5_6->SDCMR=  (8-1)<<5         // NRFS=8 SDRAM datasheet says
                                          // "at least two AUTO REFRESH cycles"
                       | FMC_SDCMR_CTB2   // Enable bank 2
                       | 3;               // MODE=011 auto refresh
    sdramCommandWait();




    FMC_Bank5_6->SDCMR=0x220<<9           // MRD=0x220:CAS latency=2 burst len=1
                       | FMC_SDCMR_CTB2   // Enable bank 2
                       | 4;               // MODE=100 load mode register
    sdramCommandWait();




    // 64ms/4096=15.625us
    #ifdef SYSCLK_FREQ_180MHz
    //15.625us*90MHz=1406-20=1386
    FMC_Bank5_6->SDRTR=1386<<1;
    #elif defined(SYSCLK_FREQ_168MHz)
    //15.625us*84MHz=1312-20=1292
    //FMC_Bank5_6->SDRTR=1292<<1;
    //in my memory 15.6
    FMC_Bank5_6->SDRTR=1290<<1;
    #else
    #error No refresh timings for this clock
    #endif
}

Outcomes