AnsweredAssumed Answered

[Solved] STM32CubeMX generated code USB Host problem

Question asked by Ivan Kuznetsov on May 7, 2015
Hello! I'm using a STM32CubeMX v4.7.1. I need to support a USB HOST MSD class in my application. So, i've included USB HOST IP, selected a peripheral and generated IAR project. I've tried to run it with USB flash drive with no success. But after editing a #define USBH_MAX_SIZE_CONFIGURATION  to 512, the HOST started to work. STM32CubeMX don't allows to edit this value more than 255.

Outcomes