AnsweredAssumed Answered

CubeMX, template for other Ethernet Phy

Question asked by Peter on May 3, 2015
Latest reply on Oct 12, 2015 by Amel N
Hi, I have an Olimex E407 Board with STM32F407ZG and PHY LAN8710A. If I make a Project in CubeMX the stm32f4xx_hal_conf.h is generated for DP83848 PHY from stm32f4xx_hal_conf_template.h in Repository\STM32Cube_FW_F4_V1.5.0\Drivers\STM32F4xx_HAL_Driver\Inc . What is the correct way to make a modification for an other PHY?

The pin PA3 is connected to ETH_RMII_MDINT of LAN8710A.
But in CubeMX I can only set ETH_COL for PA3. In the GPIO Pin Configuration this is assigned to tab "Single Mapped Signals" and not to tab ETH. 
Can I modify a template to assign ETH_RMII_MDINT  to ETH and pin PA3?



Peter

Outcomes