AnsweredAssumed Answered

STM32L152 LCD driver

Question asked by farkash on Apr 16, 2015
Latest reply on Apr 16, 2015 by farkash
Hello,

I'm working on a custom board STM32l152 that include LCD (1/4 duty & 1/3 bias)
I just want to enable all signal ( 64  =  16 * 4Com ) in order to check the screen.

somehow only 1 (of 4) raw is working.
 
this is my code :
/////////////////////////////////////////////////////////////////////////////////////////////////////////////////

/*!< Enable GPIOA, GPIOB, GPIOC AHB Clocks */
      RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_GPIOB | RCC_AHBPeriph_GPIOC, ENABLE);

      //Segments 0 - 4
      GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_LCD);
      GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_LCD);
      GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_LCD);
      GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_LCD);
      GPIO_PinAFConfig(GPIOA, GPIO_PinSource7, GPIO_AF_LCD);
     
      //Segments 5 - 6
      GPIO_PinAFConfig(GPIOC, GPIO_PinSource4, GPIO_AF_LCD);
      GPIO_PinAFConfig(GPIOC, GPIO_PinSource5, GPIO_AF_LCD);
     
           
      //Segments 7 - 8
      GPIO_PinAFConfig(GPIOB, GPIO_PinSource0, GPIO_AF_LCD);
      GPIO_PinAFConfig(GPIOB, GPIO_PinSource1, GPIO_AF_LCD);
     
       //Segments 9 - 12
      GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_LCD);
      GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_LCD);
      GPIO_PinAFConfig(GPIOC, GPIO_PinSource8, GPIO_AF_LCD);
      GPIO_PinAFConfig(GPIOC, GPIO_PinSource9, GPIO_AF_LCD);
      
     
      //Segments 13 - 15
      GPIO_PinAFConfig(GPIOB, GPIO_PinSource14, GPIO_AF_LCD);
      GPIO_PinAFConfig(GPIOB, GPIO_PinSource13, GPIO_AF_LCD);
      GPIO_PinAFConfig(GPIOB, GPIO_PinSource15, GPIO_AF_LCD);
     
      //COM 0-3
      GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_LCD);
      GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_LCD);
      GPIO_PinAFConfig(GPIOA, GPIO_PinSource10,GPIO_AF_LCD);
      GPIO_PinAFConfig(GPIOB, GPIO_PinSource9, GPIO_AF_LCD);

     
      a_opLcdControl->m_iLcdGPIO.GPIO_Pin = GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 | GPIO_Pin_6 |
                                            GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10;
      a_opLcdControl->m_iLcdGPIO.GPIO_Speed = GPIO_Speed_40MHz;
      a_opLcdControl->m_iLcdGPIO.GPIO_Mode = GPIO_Mode_AF;
      a_opLcdControl->m_iLcdGPIO.GPIO_OType = GPIO_OType_PP;
      a_opLcdControl->m_iLcdGPIO.GPIO_PuPd = GPIO_PuPd_NOPULL;
      GPIO_Init(GPIOA, &a_opLcdControl->m_iLcdGPIO);

      a_opLcdControl->m_iLcdGPIO.GPIO_Pin = GPIO_Pin_0  | GPIO_Pin_1  |  GPIO_Pin_9 |
                                            GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15;
      GPIO_Init(GPIOB, &a_opLcdControl->m_iLcdGPIO);

      a_opLcdControl->m_iLcdGPIO.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6 | GPIO_Pin_7 |
                                            GPIO_Pin_8 | GPIO_Pin_9;
      GPIO_Init(GPIOC, &a_opLcdControl->m_iLcdGPIO);

     // LCD_GPIOConfig(); /*!< Configure the LCD Glass GPIO pins */

      /*!< Configure the LCD interface -------------------------------------------*/
      RCC_APB1PeriphClockCmd(RCC_APB1Periph_LCD, ENABLE); /*!< Enable LCD APB1 Clock */
     
      a_opLcdControl->m_iLcdInit.LCD_Prescaler = LCD_Prescaler_8;//LCD_Prescaler_8;
      a_opLcdControl->m_iLcdInit.LCD_Divider = LCD_Divider_16;
      a_opLcdControl->m_iLcdInit.LCD_Duty = LCD_Duty_1_4;
      a_opLcdControl->m_iLcdInit.LCD_Bias = LCD_Bias_1_3;
      a_opLcdControl->m_iLcdInit.LCD_VoltageSource = LCD_VoltageSource_Internal;//LCD_VoltageSource_External;//LCD_VoltageSource_Internal;
      LCD_Init(&a_opLcdControl->m_iLcdInit);

      /*!< Configure the Pulse On Duration */
      LCD_PulseOnDurationConfig(LCD_PulseOnDuration_2);
     
      /*!< Configure the LCD Contrast (3.51V) */
      LCD_ContrastConfig(LCD_Contrast_Level_7);

      /*!< Wait Until the LCD FCR register is synchronized */
      LCD_WaitForSynchro();
     
      /*!< Enable LCD peripheral */
      LCD_Cmd(ENABLE);
     
      /*!< Wait Until the LCD is enabled */
      while(LCD_GetFlagStatus(LCD_FLAG_ENS) == RESET)
      {
      }
      /*!< Wait Until the LCD Booster is ready */ 
      while(LCD_GetFlagStatus(LCD_FLAG_RDY) == RESET)
      {
      }   

LCD_Write(LCD_RAMRegister_0, 0xffffffff);

LCD_UpdateDisplayRequest();     
     
////////////////////////////////////////////////////////////////////////////////////////////////////////////////

Please advise, what wrong ?

Thanks,
Moran.

Outcomes