AnsweredAssumed Answered

Editing variables during debugging...

Question asked by magalski.marcin on Apr 8, 2015
Latest reply on Apr 8, 2015 by Clive One
Hi!

I am using the stm32f429zi board and compiling it on CooCox 1.7.7 and I am a beginner in embedded programming...

During the debugging of my project, the debugger cannot see changes in variables and shows them as zeros (this variables are also not-editable)... Some variables are editable (which has lower addresses) but above some address, which I don't know, they cannot be changed...
Application works correct with this variables because they are displayed on the LCD... I don't know why the debugger can't see values of some variables...

Is it possible to fix it...? What can I do...?

Thanks a lot for any hints,

best regards,

Marcin

Outcomes