AnsweredAssumed Answered

Image Capture using STM32F2

Question asked by jain.abhilasha on Mar 27, 2015
Latest reply on Mar 27, 2015 by Clive One
I have developed a stm32f207 board for my own application. I have interfaced a 14 bit grayscale camera using DCMI. I'm then transferring this image to the SRAM using DMA. 

The SRAM being used is the same present on the stm32f220-g eval board. And I'm using ST's eval board library function for FSMC initialisation. 

Once the entire image (640 * 512) is in the SRAM, I transfer it to the PC and display it using MATLAB. The images look like this;
pcb_image1.jpg
pcb_image2.jpgAs observed, there's shift after every few lines and even though it looks like the image is there it's not quite correct.

Could someone guide me where things are going wrong? 

Outcomes