AnsweredAssumed Answered

Program STM32F103 on a SPBT2632C1A bluetooth board

Question asked by perardel.jean on Mar 12, 2015
Latest reply on Mar 12, 2015 by Clive One
Hi, 

I am planing to build a project based on a ST SPBT2632C1A. This board has a STM32F103 chip and a STLC2690 (bluetooth). If i refer to the ST document : "Comprehensive User Guide - Bluetooth classic 3.0 Modules" on page 11. 

It seems that i need an external STM32F to send AT command to the SPBT2632C1A module. Why can't I use directly the one on board? The 6 pins JTAG interface seems available (Page 6), so i should be able to program my on board chip (but probably i will have to erase an actual firmware on the STM32 no?)

I am really stock in this, it seems that the bluetooth section of the forum doesn't answer question about the ST SPBT2632 module... 

Thanks for your help :) 

Outcomes