AnsweredAssumed Answered

how to output 5V to GPOIA instead of 3.3V

Question asked by muchowski.nathan on Dec 16, 2011
Latest reply on Jul 10, 2013 by rocketdawg
I have and LCD screen that requires a positive threshold of 3.5 volts for logic high and the discovery board is only putting out 3.3V for high is there a way to change this on the board or will i need just to add some other hardware to shift the logic level to 5 volts

Outcomes