AnsweredAssumed Answered

ARM GNU Eclipse plugin and SPL

Question asked by Lukasz Przenioslo on Jan 28, 2015
Latest reply on Jan 28, 2015 by Lukasz Przenioslo
Hello there,
I am using eclipse and arm gnu eclipse plugin. It comes with HAL instead of SPL. Most of the available examples out there are SPL and I need to rely on that as I am a begginer in STM32 world. So i tried to add the SPL to my project from here:
http://www.st.com/web/en/catalog/tools/PF257901
I am using stm32f4discovery board. The problem is now that I cannot compile the code anymore as I am missing symbols. For example it says that i have no CRYP... symbols. I have looked into the stm32f407vg datasheet and it seemd that there is no CRYP module for it. I dont know why didnt it ignore it then but ok, I have removed the CRYP files. Then the same happened with DMA2 and FLASH and that I believe is present in this mcu...
I Would really aprichiate if someone could help me configuring SPL for ARM gnu eclipse enviroment. I have removed the USE_HAL symbol.

Outcomes