AnsweredAssumed Answered

WWDG IRQ firing when not confuigured

Question asked by dufrane.marcus on Dec 22, 2014
Latest reply on Dec 23, 2014 by Clive One
I have an application that I am porting from the Kiel IDE to build with the GNU tool chain. The compiled and linked appilcation on the GNU side is crashing and getting stuck in the WWDG_IRQHandler routine, though the WWDG is not currently being used. Can anyone shed some light as to what may be happening here? 

Let me know any other information you may need me to give.

The only difference I can think of besides the compiler would be that I needed to use a different linker file, however the one used by the keil compiler is the default provided by STM as is the one Im using for the GNU side.

DEVICE: stm32f103 
gnu startup file for md devices.

Outcomes