AnsweredAssumed Answered

F407 USB HS host with internal PHY

Question asked by shen.cheng on Nov 13, 2014
Latest reply on Nov 13, 2014 by Clive One
I'm using USB HS host mode with internal PHY but get a problem that i can't enter the interrupt when i plug or unplug my usb device. my program code is modified from host_device_libV2.10-USB_host_example. i just modified some init code:


i already defined USE_EMBEDDED_PHY marco and there are init code:
 USBH_Init(&USB_OTG_Host,
          USB_OTG_HS_CORE_ID, 
          &USB_Host, 
          &USBH_MSC_cb,
          &USR_Callbacks);

void USB_OTG_BSP_Init(USB_OTG_CORE_HANDLE *pdev)
{

  GPIO_InitTypeDef GPIO_InitStructure;   
  RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOB , ENABLE);  
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15 | 
                                GPIO_Pin_14;
  
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
  GPIO_Init(GPIOB, &GPIO_InitStructure);  
  
  GPIO_PinAFConfig(GPIOB,GPIO_PinSource15,GPIO_AF_OTG2_FS) ; 
  GPIO_PinAFConfig(GPIOB,GPIO_PinSource14,GPIO_AF_OTG2_FS) ;
 
  RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);
  RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_OTG_HS, ENABLE) ;
}
 

Outcomes