AnsweredAssumed Answered

STM32F401RE IAP

Question asked by Majerle.Tilen on Oct 18, 2014
Latest reply on Oct 19, 2014 by Clive One
Hi.

I'm developing an application where I have to use IAP.
I downloaded IAP example from this site and for F407VG it worked just great.

But then problems occured.
I need this on STM32F401RE. 

IAP file is uploaded to stm, everything configured.
But when I try to download file from computer (.bin) to STM via USART it says that "Verification failed". 
I'm trying this in hyperterminal v7 and Ymodem protocol.

USART is working on IAP, because I got answer from chip and I can successfully press "1", which mean "Download .bin to STM".

What are main differences between this two cips? What I need to modify in program?

Thanks for answers

Outcomes