AnsweredAssumed Answered

PMSM Vector Control (FOC) code size limit?

Question asked by Machfax on Oct 8, 2014
Latest reply on Oct 11, 2014 by jj.sprague
Hi

I'm working with an STM32F407 and the IAR embedded workbench.
I use the PMSM Vector Control Library from ST and was working with the 32kB code Size limited IAR Embedded Workbench. Now I'm working on an other system without code size limit, and if I compile the project with revuild all I get the same Error with the Code size limit. Are the Library CodeSize Limited? How can I work with the ST Librarys without code size limit? Do I have to compile them with a code size free version? But how? I^m really in troble so if anyone has any idea please post it.

Best Regards

Outcomes