AnsweredAssumed Answered

STM32 F0: Double buffered auto loaded (glitch free) PWM

Question asked by Seveelavanan.Ravicha on Oct 2, 2014
Latest reply on Oct 2, 2014 by knik
Hi,

I'm wondering if following feature exists on the any of the cheaper STM32 ranges? (e.g. STM32 F0?)...

For PWM, the duty cycle is CCRx, the value of which is compared to the counter/timer (CNT), which can be configured to toggle a pin etc. But is there any buffer for CCRx so that its value can be automatically updated at the end of each duty cycle? This is needed for perfect PWM.

Failing some auto loading buffer as above, I'm sure this can be attempted with an interrupt. However, this means that there will be an min_duty_cycle > 0% or max_duty_cycle < 100%, as the interrupt would take X cycles to complete.

Thanks 

Outcomes