AnsweredAssumed Answered

ST-LINK/V2 vs stm32f4discovery?

Question asked by belomutskiy.andrey on Sep 13, 2014
Latest reply on Sep 30, 2014 by nouha
I am having troubles setting up IAR Function Profiler so I wanted to double-check:

The grey "ST-LINK/V2" device vs the debug interface within discovery board. Are these the same exact thing? At least my Windows displays both as STlink dongle.

I have "normal" breakpoints working with IAR debugger but I cannot figure out how to get Function Profiler functioning. The UI there is... special. What CPU clock does SWO configuration window refer to - is that 168MHz in my case or is if the CPU clock of the debugger? Would it be the default 72MHz? What else can I be missing?

Outcomes