AnsweredAssumed Answered

FSMC WR behavior

Question asked by meeh.ralf on Sep 12, 2014
In a nearly ready project i wanted to add some more types of TFT displays. Now i´ve got one with an SSD1298 controller, for which well working init-code is available. I connected it in well known manner to the FSMC and it happened NOTHING...Studying the documantation of the display in precision i see: WR ist Write signal, active at Rising edge !!! So my problem is that the FSMC provides an active low Signal. Is it possible to change this behavior? I would not like to put additional hardware to the ready project. Has someone an idea? Thanks

Outcomes