AnsweredAssumed Answered

SRAM_DataMemory Issue

Question asked by abraham.nick on Aug 13, 2014
Latest reply on Aug 18, 2014 by abraham.nick
Hi,
I am unable to run the example STM32F10x_StdPeriph_Lib_V3.5.0\Project\STM32F10x_StdPeriph_Examples\FSMC\SRAM_DataMemory on my STM3210E-EVAL Board. Although I have made the following settings
       
  • Project->Options for Target window, select 'RAM1'and enter 0x68000000as start address with size of 0x100000 (IRAM1 must be un-checked)
       
  • uncomment "#define DATA_IN_ExtSRAM " in the "system_stm32f10x.c" file

But still the code is unable to execute. Attached zip file is the complete project folder.

regards,
Nick.

Attachments

Outcomes