AnsweredAssumed Answered

Unable to read file greater than 2K in FatFS ,stm32F103

Question asked by ak.c on Aug 11, 2014
Latest reply on Aug 14, 2014 by ak.c

Hi,
I am reading a file from the SPI Flash with FATFS file system, on STM32F103 platform running FreeRTOS. I can successfully read File of size less the 2048, but if read a file file of size greater than 2048, (As i am reading in chunks of 128 bytes) it only reads up to 2048 bytes and f_read returns 'FR_INT_ERR' error when File pointer move to location above 2048 bytes.

Thanking in an anticipation,

CAK

Outcomes