AnsweredAssumed Answered

Wakeup from SPI question

Question asked by ofri.igal on Jun 29, 2014
Latest reply on Jul 2, 2014 by ofri.igal
I would like to wake up from SPI communication (using the NSS pin).

I have the NSS line connected to both PA0 and the SPI(3) NSS pin.

I would like to wake up from either stop mode or stanby mode (preferably standby mode) while not loosing the data sent to me. is that possible? if so, how?

I'm running STM32F405, at 84MHz.

I know it is possible in other M4 core processor but couldn't figure out how to do it in this one.

Thank you

Outcomes