AnsweredAssumed Answered

Send 64 bytes to xbee pro S2b & send to sleep mode

Question asked by A2 on Jun 27, 2014
Hi,

I need to transmit 64 bytes at a time with xbee-pro-s2b. Then send xbee into sleep since this is battery powered application.

At receiver end another xbee-pro-2b is connected which is not battery powered. So always on.



At transmitter side power is a issue, so I want to send 64 bytes at a time & then set Sleep pin high.

xbee pin will tx all the 64 bytes & go to sleep afterwards.



Is there any example code for this??

Outcomes