AnsweredAssumed Answered

Pilot LEDs: problem

Question asked by hibou.geo on Jun 8, 2014
I want to pilot LED on a ws2812: here is the datasheet
http://www.adafruit.com/datasheets/WS2812.pdf

Like you can see you need 24 bits for pilot one LED (change the color) ..My LEDs are only white every time ... I don't understand why because my table Led_Byte_Buffer is correct (I saw it whith the debug) and my times too (350ns for a 0 and 700ns for a 1).

Help please

Here the code:

#include "main.h"
#include "usbd_hid_core.h"
#include "usbd_usr.h"
#include "usbd_desc.h"
  
  
#define TESTRESULT_ADDRESS         0x080FFFFC
#define ALLTEST_PASS               0x00000000
#define ALLTEST_FAIL               0x55555555
  
//#define TIM3_CCR1_Address 0x40000434        // physical memory address of Timer 3CCR1 register
#define d2r (3.14159265/180)
  
 
#ifdef USB_OTG_HS_INTERNAL_DMA_ENABLED
  #if defined ( __ICCARM__ ) /*!< IAR Compiler */
    #pragma data_alignment = 4
  #endif
#endif /* USB_OTG_HS_INTERNAL_DMA_ENABLED */
__ALIGN_BEGIN USB_OTG_CORE_HANDLE  USB_OTG_dev __ALIGN_END;
  
uint16_t PrescalerValue = 0;
  
__IO uint32_t TimingDelay;
__IO uint8_t DemoEnterCondition = 0x00;
__IO uint8_t UserButtonPressed = 0x00;
LIS302DL_InitTypeDef  LIS302DL_InitStruct;
LIS302DL_FilterConfigTypeDef LIS302DL_FilterStruct;
__IO int8_t X_Offset, Y_Offset, Z_Offset  = 0x00;
uint8_t Buffer[6];
 
        uint8_t led;
        uint16_t memaddr;
  
  
TIM_TimeBaseInitTypeDef  TIM_TimeBaseStructure;
TIM_OCInitTypeDef  TIM_OCInitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
DMA_InitTypeDef DMA_InitStructure1;
  
uint16_t LED_BYTE_Buffer[240];
  
uint8_t eightbit[766][3] =
{
        {255, 0, 0},
    {254, 1, 0},
    //...... BIG TABLE
    {253, 0, 2},
    {254, 0, 1},
    {255, 0, 0},
};
  
  
 
 
  
  
void Timer3_init(void)
{
        uint16_t PrescalerValue;
  
        RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
        GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;
        GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
        GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
        GPIO_Init(GPIOC, &GPIO_InitStructure);
  
        GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_TIM3);
  
        RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
        /* Compute the prescaler value */
        PrescalerValue = (uint16_t) (SystemCoreClock / 168000000) - 1;
        /* Time base configuration */
        TIM_TimeBaseStructure.TIM_Period = 105; // 800kHz
        TIM_TimeBaseStructure.TIM_Prescaler = PrescalerValue;
        TIM_TimeBaseStructure.TIM_ClockDivision = 0;
        TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
        TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
  
        TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
        TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
        TIM_OCInitStructure.TIM_Pulse = 0;
        TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
        TIM_OC1Init(TIM3, &TIM_OCInitStructure);
  
        /* configure DMA */
        /* DMA clock enable */
        RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA1, ENABLE);
  
  
        DMA_DeInit(DMA1_Stream4);
  
          /* Configure DMA Stream */
  DMA_InitStructure1.DMA_Channel = DMA_Channel_5;
  DMA_InitStructure1.DMA_PeripheralBaseAddr = (uint32_t)&TIM3->CCR1;
  DMA_InitStructure1.DMA_Memory0BaseAddr = (uint32_t)LED_BYTE_Buffer;
  DMA_InitStructure1.DMA_DIR = DMA_DIR_MemoryToPeripheral;
  DMA_InitStructure1.DMA_BufferSize = 1;
  DMA_InitStructure1.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
  DMA_InitStructure1.DMA_MemoryInc = DMA_MemoryInc_Disable;
  DMA_InitStructure1.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
  DMA_InitStructure1.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
  DMA_InitStructure1.DMA_Mode = DMA_Mode_Normal;
  DMA_InitStructure1.DMA_Priority = DMA_Priority_High;
  DMA_InitStructure1.DMA_FIFOMode = DMA_FIFOMode_Disable;
  //DMA_InitStructure1.DMA_FIFOThreshold = DMA_FIFOThreshold_Full;
    //DMA_InitStructure1.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
    //DMA_InitStructure1.DMA_MemoryBurst = DMA_MemoryBurst_Single;
  //DMA_InitStructure1.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
  DMA_Init(DMA1_Stream4, &DMA_InitStructure1);
  
         /* TIM3 CC1 DMA Request enable */
        TIM_DMACmd(TIM3, TIM_DMA_CC1, ENABLE);
}
  
void WS2812_send(uint8_t (*color)[3], uint16_t len)
{
        uint8_t j;
 
        uint16_t buffersize;
                int zero = 30;
                int un = 60;
         
  
        buffersize = (len*24);        // number of bytes needed is #LEDs * 24 bytes +42 trailing bytes
        memaddr = 0;                                // reset buffer memory index
        led = 0;                                        // reset led index
  
        // fill transmit buffer with correct compare values to achieve
        // correct pulse widths according to color values
        while (len)
        {
 
                 
 
                for (j = 0; j < 8; j++)                                        // GREEN data
                {
                        if ( (color[led][0]<<j) & 0x80)        // data sent MSB first, j = 0 is MSB j= 7 is LSB
                        {
                                LED_BYTE_Buffer[memaddr] = un;         // compare value for logical 1
                        }
                        else
                        {
                                LED_BYTE_Buffer[memaddr] = zero;        // compare value for logical 0
                        }
                        memaddr++;
                }
  
                for (j = 0; j < 8; j++)                                        // RED data
                {
                        if ( (color[led][1]<<j) & 0x80 )        // data sent MSB first, j = 0 is MSB j= 7 is LSB
                        {
                                LED_BYTE_Buffer[memaddr] = un;         // compare value for logical 1
                        }
                        else
                        {
                                LED_BYTE_Buffer[memaddr] = zero;        // compare value for logical 0
                        }
                        memaddr++;
                }
  
                for (j = 0; j < 8; j++)                                        // BLUE data
                {
                        if ( (color[led][2]<<j) & 0x80 )        // data sent MSB first, j = 0 is MSB j= 7 is LSB
                        {
                                LED_BYTE_Buffer[memaddr] = un;         // compare value for logical 1
                        }
                        else
                        {
                                LED_BYTE_Buffer[memaddr] = zero;        // compare value for logical 0
                        }
                        memaddr++;
                }
  
                led++;
                len--;
        }
  
        // add needed delay at end of byte cycle, pulsewidth = 0
        while(memaddr < buffersize)
        {
                LED_BYTE_Buffer[memaddr] = 0;
                memaddr++;                 
                }
         
  
        DMA_SetCurrDataCounter(DMA1_Stream4, buffersize);
        DMA_Cmd(DMA1_Stream4, ENABLE);
        TIM_Cmd(TIM3, ENABLE);
        while(!DMA_GetFlagStatus(DMA1_Stream4, DMA_FLAG_TCIF4));       
        TIM_Cmd(TIM3, DISABLE);                                    
        DMA_Cmd(DMA1_Stream4, DISABLE);              
                DMA_ClearFlag(DMA1_Stream4, DMA_FLAG_TCIF4);
}
  
int main(void)
{
        int16_t i;
        Timer3_init();
 
  
  
  
  
  
        while (1){
                /* first cycle through the colors on 2 LEDs chained together
                 * last LED in the chain will receive first sent triplet
                 * --> last LED in the chain will 'lead'
                 */
                     
                for (i = 0; i < 700; i += 1)
                {
                        WS2812_send(&eightbit[i], 5);
                                                Delay(40000L);
                }
 
                                 
                                 
  
                /* cycle through the colors on only one LED
                 * this time only the first LED that data is
                 * fed into will update
                 */
              /*  for (i = 0; i < 766; i += 1)
                {
                        WS2812_send(&eightbit[i], 2);
                               // Delay(50000L);
                }*/
        }
}
  
  
  
void Delay(__IO uint32_t nTime)
{
  TimingDelay = nTime;
  
  while(TimingDelay != 0) TimingDelay--;
}
  
/**
  * @brief  Decrements the TimingDelay variable.
  * @param  None
  * @retval None
  */
void TimingDelay_Decrement(void)
{
  if (TimingDelay != 0x00)
  {
    TimingDelay--;
  }
}
  
/**
  * @brief  This function handles the test program fail.
  * @param  None
  * @retval None
  */
void Fail_Handler(void)
{
  /* Erase last sector */
  FLASH_EraseSector(FLASH_Sector_11, VoltageRange_3);
  /* Write FAIL code at last word in the flash memory */
  FLASH_ProgramWord(TESTRESULT_ADDRESS, ALLTEST_FAIL);
  
  while(1)
  {
    /* Toggle Red LED */
    STM_EVAL_LEDToggle(LED5);
    Delay(5);
  }
}
  
/**
  * @brief  MEMS accelerometre management of the timeout situation.
  * @param  None.
  * @retval None.
  */
uint32_t LIS302DL_TIMEOUT_UserCallback(void)
{
  /* MEMS Accelerometer Timeout error occured during Test program
execution */
  if (DemoEnterCondition == 0x00)
  {
    /* Timeout error occured for SPI TXE/RXNE flags waiting loops.*/
    Fail_Handler();
  }
  /* MEMS Accelerometer Timeout error occured during Demo execution */
  else
  {
    while (1)
    {
    }
  }
  return 0;
}
  
#ifdef  USE_FULL_ASSERT
  
/**
  * @brief  Reports the name of the source file and the source line number
  *   where the assert_param error has occurred.
  * @param  file: pointer to the source file name
  * @param  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t* file, uint32_t line)
{
  /* User can add his own implementation to report the file name and line
number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file,
line) */
  
  /* Infinite loop */
  while (1)
  {
  }
}
#endif

Outcomes