AnsweredAssumed Answered

STM32F205 DCMI

Question asked by krueger.thomas on May 15, 2014
Latest reply on May 16, 2014 by Clive One
Hello Forum,

I do have a STM32F205VE device 100Pin Package to which i connected a Camera as to the DCMI Interface.

From the DCMI Status register i can tell, that HSYNC and VSYNC are detected.

However, nothing is captured.

The PXCLK  (Pixelclock) is routed to PA6  (AF=DCMI PXCLK).

Somewhere in the datasheet i now red that DCMI is not supported on STMF205 devices.

Is that true?

It seems that PA6 (Pixelclock) is not reaching the DCMI module allthough present on the Pin.

Thanks.


Outcomes