AnsweredAssumed Answered

How to retrieve 8MHz from 168 MHz processor

Question asked by sminder on Apr 11, 2014
Latest reply on Apr 15, 2014 by Clive One
I've got STM32F407VE controller that works at 168 MHz. I need to get a 8 MHz clock frequency from it and I guessed to use a timer in PWM mode, but they all have a 42 MHz or 84 MHz clocks and so I can't use approriate divider for desired frequency. How can I get this frequency from the controller?

Oops, sorry. It is just an clock frequency to timer's periphery and I can use a half of CPU working frequency. I just ran the controller on 160 MHz and it looks well.

Outcomes