AnsweredAssumed Answered

STM32 Cryptographic Library

Question asked by wainshtein.boris on Apr 9, 2014
Hi,

I am using  STM32 Cryptographic Library . There is a function "STM32_CryptoLibraryVersion" that gets as a parameter the
structure  STM32CryptoLibVer_TypeDef.

The problem is that I can't find the description about the elements of this structure
not in document UM0586 and not in source code.

I am interesting in "uint8_t T[2]; " parameter description.

Do someone can help me ?

typedef

 

 

 

 

struct </p>

 

</b>

{

 

uint8_t X; /*!< Used to get the X parametre of the current STM32 crypto library verion */

 

 

uint8_t Y; /*!< Used to get the Y parametre of the current STM32 crypto library verion */

 

 

uint8_t Z; /*!< Used to get the Z parametre of the current STM32 crypto library verion */

 

 

uint8_t T[2]; /*!< Used to get the Type of the verion. This parametre can be "HW" or "FW" */

 

 

uint8_t CortexConf ;

 

 

uint8_t MicroConf ;

 

 

uint8_t EndiannessConf ;

 

 

uint8_t MisalignedConf ;

 

 

uint8_t EncDecConf;

 

 

uint16_t SymKeyConf ;

 

 

uint16_t SymKeyModesConf ;

 

 

uint16_t AsymKeyConf ;

 

 

uint16_t HashConf ;

 

 

uint8_t DrbgConf ;

 

 

uint8_t AesConf ;

 

 

uint8_t RsaConf ;

 

 

uint8_t GcmConf ;

 

 

}

STM32CryptoLibVer_TypeDef;

 


Outcomes