AnsweredAssumed Answered

Jump address to choose one of 2 binary in flash

Question asked by Tom_Rfid on Apr 3, 2014
Latest reply on Apr 10, 2014 by Tom_Rfid
Hello,

I'm trying to create a bootloader into the component STM32f106RDT with 384KO of Flash.
I have mapped the memory like this:
0x08000000 - 0x0802DFFF for main software (first binary)
0x0802F000 - 0x08030FFF reserved
0x08031000 - 0x0805FFFF for the temp binary (second binary)

My function of bootloader() to jump at selected main address is in flash.
When I debug with keil the pc is in the file startup_stm32f10x_hd.s, then i want to go into my function bootloader so IMPORT the function like this :


; Reset handler
Reset_Handler   PROC
                EXPORT  Reset_Handler             [WEAK]
                IMPORT  __main
                IMPORT  SystemInit
                IMPORT  FLASH_Bootloader       /*my add*/
                LDR     R0, =SystemInit
                BLX     R0              
                LDR     R0, =FLASH_Bootloader  /*my add*/
                BLX     R0                                       /*my add*/
                ;LDR     R0, =__main
                ;BX      R0
                ENDP


The problem is that i want to jump on one of the two binary file. How do i get the flash address of the main() function? If i jump on 0x08000000+4 the beginning of the first binary mapping it does nothing.
Somebody have an idea to select one of my 2 apps and run it?

Thank you.

Outcomes