AnsweredAssumed Answered

HEEEEEELP With FSMC SRAM interface

Question asked by t.muhammad on Feb 19, 2014
Latest reply on Feb 20, 2014 by t.muhammad
I have been struggling for 3 days now to get this interface working and write to SRAM properly , but this is not working still , Here is the code i used.
int main(void)
{
  SRAM_Init();
  while (1)
  {
            *(uint16_t *) (0x64000000)=0xAADD; // break point here
  }
}
//
//
//

void SRAM_Init(void)
{
  FSMC_NORSRAMInitTypeDef  FSMC_NORSRAMInitStructure;
  FSMC_NORSRAMTimingInitTypeDef  p;
  GPIO_InitTypeDef GPIO_InitStructure;
 
  /* Enable GPIOs clock */
  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD | RCC_AHB1Periph_GPIOE | RCC_AHB1Periph_GPIOF |
                         RCC_AHB1Periph_GPIOG, ENABLE);

  /* Enable FSMC clock */
  RCC_AHB3PeriphClockCmd(RCC_AHB3Periph_FSMC, ENABLE);
 
/*-- GPIOs Configuration ------------------------------------------------------*/
/*
 +-------------------+--------------------+------------------+------------------+
 +                       SRAM pins assignment                                  +
 +-------------------+--------------------+------------------+------------------+
 | PD0  <-> FSMC_D2  | PE0  <-> FSMC_NBL0 | PF0  <-> FSMC_A0 | PG0 <-> FSMC_A10 |
 | PD1  <-> FSMC_D3  | PE1  <-> FSMC_NBL1 | PF1  <-> FSMC_A1 | PG1 <-> FSMC_A11 |
 | PD4  <-> FSMC_NOE | PE7  <-> FSMC_D4   | PF2  <-> FSMC_A2 | PG2 <-> FSMC_A12 |
 | PD5  <-> FSMC_NWE | PE8  <-> FSMC_D5   | PF3  <-> FSMC_A3 | PG3 <-> FSMC_A13 |
 | PD8  <-> FSMC_D13 | PE9  <-> FSMC_D6   | PF4  <-> FSMC_A4 | PG4 <-> FSMC_A14 |
 | PD9  <-> FSMC_D14 | PE10 <-> FSMC_D7   | PF5  <-> FSMC_A5 | PG5 <-> FSMC_A15 |
 | PD10 <-> FSMC_D15 | PE11 <-> FSMC_D8   | PF12 <-> FSMC_A6 | PG9 <-> FSMC_NE2 |
 | PD11 <-> FSMC_A16 | PE12 <-> FSMC_D9   | PF13 <-> FSMC_A7 |------------------+
 | PD12 <-> FSMC_A17 | PE13 <-> FSMC_D10  | PF14 <-> FSMC_A8 |
 | PD14 <-> FSMC_D0  | PE14 <-> FSMC_D11  | PF15 <-> FSMC_A9 |
 | PD15 <-> FSMC_D1  | PE15 <-> FSMC_D12  |------------------+
 +-------------------+--------------------+
*/
  /* GPIOD configuration */
  GPIO_PinAFConfig(GPIOD, GPIO_PinSource0, GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOD, GPIO_PinSource1, GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOD, GPIO_PinSource4, GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOD, GPIO_PinSource5, GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOD, GPIO_PinSource10, GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOD, GPIO_PinSource11, GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOD, GPIO_PinSource12, GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOD, GPIO_PinSource14, GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOD, GPIO_PinSource15, GPIO_AF_FSMC);

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_4 | GPIO_Pin_5 |
                                GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 |
                                GPIO_Pin_12 | GPIO_Pin_14 | GPIO_Pin_15;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
  GPIO_InitStructure.GPIO_PuPd  = GPIO_PuPd_NOPULL;

  GPIO_Init(GPIOD, &GPIO_InitStructure);


  /* GPIOE configuration */
  GPIO_PinAFConfig(GPIOE, GPIO_PinSource0 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOE, GPIO_PinSource1 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOE, GPIO_PinSource7 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOE, GPIO_PinSource8 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOE, GPIO_PinSource9 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOE, GPIO_PinSource10 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOE, GPIO_PinSource11 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOE, GPIO_PinSource12 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOE, GPIO_PinSource13 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOE, GPIO_PinSource14 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOE, GPIO_PinSource15 , GPIO_AF_FSMC);

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0  | GPIO_Pin_1 | GPIO_Pin_7 |
                                GPIO_Pin_8  | GPIO_Pin_9  | GPIO_Pin_10 | GPIO_Pin_11|
                                GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15;

  GPIO_Init(GPIOE, &GPIO_InitStructure);


  /* GPIOF configuration */
  GPIO_PinAFConfig(GPIOF, GPIO_PinSource0 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOF, GPIO_PinSource1 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOF, GPIO_PinSource2 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOF, GPIO_PinSource3 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOF, GPIO_PinSource4 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOF, GPIO_PinSource5 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOF, GPIO_PinSource12 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOF, GPIO_PinSource13 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOF, GPIO_PinSource14 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOF, GPIO_PinSource15 , GPIO_AF_FSMC);

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0  | GPIO_Pin_1  | GPIO_Pin_2  | GPIO_Pin_3 |
                                GPIO_Pin_4  | GPIO_Pin_5  |
                                GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15;      

  GPIO_Init(GPIOF, &GPIO_InitStructure);


  /* GPIOG configuration */
  GPIO_PinAFConfig(GPIOG, GPIO_PinSource0 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOG, GPIO_PinSource1 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOG, GPIO_PinSource2 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOG, GPIO_PinSource3 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOG, GPIO_PinSource4 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOG, GPIO_PinSource5 , GPIO_AF_FSMC);
  GPIO_PinAFConfig(GPIOG, GPIO_PinSource9 , GPIO_AF_FSMC);

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0  | GPIO_Pin_1  | GPIO_Pin_2  | GPIO_Pin_3 |
                                GPIO_Pin_4  | GPIO_Pin_5  |GPIO_Pin_9;      

  GPIO_Init(GPIOG, &GPIO_InitStructure);

/*-- FSMC Configuration ------------------------------------------------------*/
  p.FSMC_AddressSetupTime = 5;
  p.FSMC_AddressHoldTime = 0;
  p.FSMC_DataSetupTime = 5;
  p.FSMC_BusTurnAroundDuration = 0;
  p.FSMC_CLKDivision = 0;
  p.FSMC_DataLatency = 0;
  p.FSMC_AccessMode = FSMC_AccessMode_A;

  FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM2;
  FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable;
  FSMC_NORSRAMInitStructure.FSMC_MemoryType = FSMC_MemoryType_SRAM;
  FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_16b;
  FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode = FSMC_BurstAccessMode_Disable;
  FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low;
  FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable;
  FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState;
  FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable;
  FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable;
  FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Disable;
  FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable;
  FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &p;
  FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &p;

  FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure);

  /*!< Enable FSMC Bank1_SRAM2 Bank */
  FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM2, ENABLE);

}
//
//
Now when i debug , i see that many addresses change , and never get the write value in place.
My SRAM chip and MCU are the same as the ones on that board but separate , so definitly they are supposed to work together.
http://www.hotmcu.com/hystm32f2xxcore144-coredev-board-p-3.html?cPath=1_20



Outcomes