AnsweredAssumed Answered

Unable to connect to hidden wireless network with SPWF01SA21 on FW3.4

Question asked by Joe on Sep 15, 2015
Latest reply on Sep 17, 2015 by Gerardo Gallucci
Hi,

I tried to connect to a wireless network, which do not broadcast its SSID, with the above mentioned module.

I tried as usual:

AT+S.SCAN
AT+S.SSIDTXT=TestAP
AT+S.SCFG=wifi_wpa_psk_text,Test123
AT+S.SCFG=wifi_priv_mode,2
AT+S.SCFG=wifi_mode,1
AT&W
AT+CFUN=1

The response after the reset is just the scanning procedure...

+WIND:2:Reset
+WIND:1:Poweron (150410-c2e37a3-SPWF02S)
+WIND:13:ST SPWF01SA2 IWM: Copyright (c) 2012-2014 STMicroelectronics...
+WIND:3:Watchdog Running
+WIND:46:WPA: Crunching PSK...
+WIND:0:Console active
+WIND:32:WiFi Hardware Started
+WIND:21:WiFi Scanning
+WIND:35:WiFi Scan Complete (0x0)

Is there something I've to add to the configuration to get it done?

Thanks

Outcomes