AnsweredAssumed Answered

STM32F439I-EVAL2 board and STM32Cube

Question asked by aiyer.kartik on Apr 15, 2014
Latest reply on May 13, 2014 by Nic D
We just bought an STM32F439I Evaluation board with the 5.7" pCap touch panel/ LCD. I would like to startup a basic template project which will actually have some of the components up and running. I would like to use the STM32Cube software to tweak this and was wondering if there is a .ioc project for the STM32F439I eval board that ST can provide so that I can load the STM32Cube program with a good reference pinout, clock, etc setttings. If not what is the best approach to go about making sure all the peripherals and pins are configured appropriately for the evaluation board? 

Also, I got a general firmware dump for STM32F4x9. This seemed to have the necessary driver code for the LCD on the 429 board, however, I'm not sure if the necessary driver code for the 5.7"LCD and touch panel is available on the 439 baord. Can someone tell me if I that driver code is part of a binary, or do we have access to that code ?

Regards
Kartik

Outcomes