AnsweredAssumed Answered

Problem with reconnect to board after power down

Question asked by tal.ram on Aug 18, 2016
Latest reply on Aug 28, 2016 by tal.ram
Hi, we're using the MB1054A board for reading ISO 15693 tags and it works OK.
the problem occurs after immediate power down- we are facing problems with initiation.
The OS on the PC is Win-10 and we're not sure the CR95HF.dll is the same used on the application SW. how come when shut down the PC and power up again, and then open again the application SW everything is working OK?
Do ST supply source code example for the PC side? 

Outcomes