AnsweredAssumed Answered

M24LR-E energy harvesting

Question asked by so.sunny on Mar 23, 2016
Latest reply on Oct 18, 2016 by NFC IC support2
I test with 24LR04e-discovery board..Use CR95HF demo board to set EH enable-03,and 
EH Config-F3. Put board near wire and the board can display message. But if I set F0 and mean max 7mA. It is very difficult to drive the board message display. I measure the VDD output and always about 0.5V. Why set max current higher not better ? How can i set to output more current to 7mA?  thanks

Outcomes