AnsweredAssumed Answered

Can I use of SPIRIT1 for MICS band(403MHz)?

Question asked by do.quyen.001 on Jan 15, 2015
Latest reply on Jan 15, 2015 by panvini.gaetano
Hi all,
I have a project in which I have to use MICS band for data telemetry in an implantable device. 
Can I use the SPIRIT1 for MICS band which centers at 403MHz? (I think the TI CC1101 can be configured to do it, so should be the same for the SPIRIT1).
If it is possible, then I guess I can still use the reference BOM for 433MHz for my design and the only thing I need to change is to configure the frequency base and center frequency to 403MHz through the Spirit1DK GUI?

I'm looking forward to hearing from you all,
Thanks
Quyen

Outcomes