AnsweredAssumed Answered

Question about STM32F4, DISCOVERY, EVAL BOARD with IAR EWARM 6.5.3

Question asked by naughty_mark on Apr 6, 2014
Latest reply on Apr 8, 2014 by Clive One
Hi everyone,

I am a newbie to arm microcontroller and STM32 product. recently I want to buy a STM32F4-Discovery Board to play with arm chip. That board uses STM32F429I arm chip, and my toolchain is IAR EWARM 6.5.3, in the project option->general, I can not find this specific chip in the list, so my question is:
1. Is that ok I use such version IAR tool to compile and make STM32F429I arm chip project?
2. If yes to question1, what do I need to select for that "target" tab in project otpion->general. What I am currently do is tick "Core" as "Cortex-M4F" rather than choose a specific device, and I can compile and make the demo project successfully, but I have no idea the hex file generated under this configuration is proper or not.

Thanks for all your time.

Kind Regards
Mark

Outcomes