AnsweredAssumed Answered

STM32CubeMX bug with STM32F030x (GPIO mode)

Question asked by Andrey.St on Apr 3, 2014
Latest reply on Jun 6, 2014 by STM32Cube-T
After upgrading to version 4.1 .
There are the following problems .

When creating a new project (MCU STM32F030F4Px) and assigning output PA0 ( tab PINOUT) as GPIO_Input, then clicking in the tab Configuration -> GPIO everything right : GPIO mode: Input mode, it is possible to select the pull up / pull down.

But as soon as we add ( tab PINOUT) PA1 pin as an analog input , the tab Configuration -> GPIO changes occur PA0 pin changes the value on the GPIO mode GPIO_Mode_In and no ability to select pull up / pull down.

And bid.
In the generated file will be twice repeated line RCC_AHBPeriphClockCmd (RCC_AHBPeriph_GPIOA, ENABLE);Is it possible when generating code to check if previously set clock ports to avoid provoking the code redundancy .

Outcomes