AnsweredAssumed Answered

Reset after firmware upgrade

Question asked by lee.n on Jan 23, 2014
Latest reply on Nov 10, 2016 by ramirez.jaime

I have used the STM32 USB-FS-Device development kit examples to implement the custom HID and the DFU. It all works OK and I can upgrade the custom HID application from the DFU application using DfuSeDemo.  The problem is that the DFU application does not reset when the upgrade is complete, I have to cycle the power. There is a system reset in the code but it isn’t called. Where do I need to do the system reset to force the DFU app to reset when the download is complete?

Outcomes