AnsweredAssumed Answered

Windows 8.1 Tablet, STLink Driver Issue

Question asked by c.adam on Jan 10, 2014
Latest reply on Jan 11, 2014 by c.adam
I cannot seem to get the STLink driver to install on my Dell Venue 8 Pro tablet.  When I try and install it gives an error.  I have made sure to "Run as Administrator" when attempting to install.  The error in the driver installation wizard is simply "Install Failed".  So I then tried to go into the device manager and force it to update the driver there.  I point it to the correct location and the error that I get is "A problem was encountered while attempting to add the driver to the store."  Does anyone have any ideas?  I am using the correct signed driver (download stsw-link006).

As to why would anyone want to use a small tablet, it is really great for when you are traveling and need to travel light.  If I can get this to work, then I will be able to do the rest of what I need to do. 

Thanks,
Adam

Outcomes