AnsweredAssumed Answered

Unable to program STM32F1x using the ST-link/openOCD

Question asked by Evert on Jan 9, 2014
Latest reply on Jan 17, 2014 by Juha Aaltonen
Hello,

I like to program my STM32F103 with the ST-link/V2 device by using openOCD.
However I got next message:

Error: flash write failed at address 0x80016f8
Error: error writing to flash at address 0x08000000 at offset 0x00000000

By using the ST-link Utility, it works fine with the same programmer.

I am using the stm32f1x_stlink.cfg target script and next openocd script for writing:
I call this script from my makefile (IMGFILE is my binary)

roc stm_flash {IMGFILE} {
 reset halt
 sleep 10
 wait_halt 2
 flash write_image erase $IMGFILE 0x08008000
 sleep 10
 verify_image $IMGFILE 0x08008000
 sleep 10
 reset run
}

Does anyone has an idea what is going on?

Regards Evert Huijben

Here is the complete logging:
make program
Open On-Chip Debugger 0.6.1 (2014-01-08-11:14)
Licensed under GNU GPL v2
For bug reports, read
 http://openocd.sourceforge.net/doc/doxygen/bugs.html
adapter speed: 1000 kHz
srst_only separate srst_nogate srst_open_drain
Info : clock speed 1000 kHz
Info : stm32f1x.cpu: hardware has 6 breakpoints, 4 watchpoints
stm_erase
target state: halted
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x08000160 msp: 0x20000400
auto erase enabled
Info : device id = 0x20036410
Info : flash size = 128kbytes
Error: flash write algorithm aborted by target
target state: halted
target halted due to breakpoint, current mode: Thread
xPSR: 0x01000000 pc: 0x08000160 msp: 0x20000400
Error: flash write failed at address 0x80016f8
Error: error writing to flash at address 0x08000000 at offset 0x00000000
Runtime Error: /home/evert/sandbox/multi_IO/projects/chibiOs/make/../../../boards/multiIo/stm32f1-openocd.cfg:12:
in procedure 'stm_flash'
in procedure 'flash' called at file "/home/evert/sandbox/multi_IO/projects/chibiOs/make/../../../boards/multiIo/stm32f1-openocd.cfg", line 12
make: Nothing to be done for `program'.


Outcomes