AnsweredAssumed Answered

Bringing up the BlueNRG device is failing!

Question asked by roby.guy on Dec 1, 2015
Latest reply on Dec 9, 2015 by roby.guy
I am using BlueNRG ver 2 device, I'm using not an ST MCU, but freescale's.
SPI was porting to my MCU Kinetis and the issue is:

Instead of getting the "Blue_Initialized_Event" (0x04, 0xff, 0x03, 0x01, 0x00, 0x01),
I'm getting (0xff, 0xff, 0xff, 0xff, 0xff, 0xff).

The first 5 bytes SPI are OK and the second 5 bytes are also OK.

(the Bring UP is according to "Bringing up the BlueNRG and BlueNRG-MS devices")

Untitled.png
attached waveform to describe the SPI signals.

Thanks in advance,
Guy

Attachments

Outcomes