AnsweredAssumed Answered

STemWin Display Orientatino

Question asked by aiyer.kartik on Jun 18, 2014
Latest reply on Nov 5, 2014 by Montassar BEN ROMDHANE
I'm working with the STM32F439_Evaluation platform. I swapped the display out with an AMP 480X272 pcap display and have everything working. I used the LCD Conf file from the demo project and made some compile time based changes for XSIZE_PHYS and YSIZE_PHYS. I want to change the orientation to a portrait scheme and changing LCD_SWAP_XY doesn't seem to do it. I don't see any references to it in the supplied LCDConf.c file leading me to believe that it is not setup for protrait orientation. Any tips on the changes I need to make to get it to work ? Are any changes needed to be made in with regards to the frame buffer allocation ?

Outcomes