AnsweredAssumed Answered

STM32F205 in STOP mode with MCO pin

Question asked by palmer.david on Oct 22, 2013
Latest reply on Oct 22, 2013 by Clive One
In the STM32F205 datasheet, it says that in STOP power mode, all clocks on the 1.2V power domain are stopped. Is there anywhere I can look to see which clocks are part of the "1.2V power domain" ?

Particularly, I'm interested if the MCO pin will continue to run in this power mode. My MCO pin has its source set to the LSE oscillator.

DP

Outcomes