AnsweredAssumed Answered

SPWF01Sx - Auto-enabling socket server at boot

Question asked by pellizzari.martino on Sep 9, 2016
Latest reply on Sep 9, 2016 by Gerardo Gallucci
I'm evaluating the SPWF01x module for use in a cable-replacement application.
What I need to do is setup the module as an AP, connect to it and switch to data mode.

Following the documentation I've already put the module in MiniAP mode, set the desired IP, enabled the DHCP server and stored all required passkeys. I've run some tests and it already works as needed (which is very good indeed) except for one thing: after a reboot of the module, the socket server is always off.

I would like to know if and how the server can be activated automatically when the module is powered on.

Thank you in advance

Outcomes