AnsweredAssumed Answered

Dead time accessed when?

Question asked by Limestone on Sep 25, 2013
Latest reply on Sep 25, 2013 by Jack Peacock
Hi

I need to be able to adjust the dead time of one of the advanced timers in an F4 during execution.
I can easily write to the BDTR register but it seems a bit dangerous to do so without knowing when the timer will use the content of the register in order to control the outputs. 

Anybody knows when this is done or perhaps if the register is shadowed during update event or something like that?

// Martin

Outcomes