AnsweredAssumed Answered

No NAND flash on STM3220G-Eval

Question asked by tze_wan.foo on Sep 13, 2013
Latest reply on Sep 20, 2013 by tze_wan.foo
Hi all,

I would like to evaluate the NAND flash interface with the STM3220G-Eval board. However, this board is not populated with the NAND flash, although the board has an estate-area for it. If I were to buy a flash, I do not have the tools to solder the BGA-type flash onto it either. Are there any ways where I can evaluate flash functionality on STM32 F2 series? I am using IAR as the compiler. I do have another STM3210E-Eval which has a populated flash. However, this board is based on F2 series, which is not what our team wants in the final design.

I would appreciate any feedback or ideas. Thanks in advance.

Outcomes