AnsweredAssumed Answered

Use of multiple analog functions of same pin possible?

Question asked by Benny on Sep 10, 2013
Latest reply on Oct 10, 2013 by Amel N
Hello guys!

I wonder if it is possible to use more than one additional function if the pin is configured as an analog input. I can not find any detail in the datasheet or reference manual that denies or allows this kind of usage especially.

For instance (see attachment): Is it possible to use PA1 as input for COMP1 and OPAMP1 on the STM32F302RC at the same time?

Attached picture (abstract of pin config in datasheet)

Thanks for your help.

Greetings,
Benny

Attachments

Outcomes