AnsweredAssumed Answered

bootloader and atollic

Question asked by pcu on Sep 5, 2013
Latest reply on Sep 7, 2013 by Clive One
Hello,

I work on the bootloader IAP_ethernet from ST.
I use the TFTP transfer.
When I use the image "Ethernet_IAP_STM3240 \ binary \ STM324xG_EVAL_SysTick.bin" provided in the example AN3376, it works correctly.

When I use the same project compiled by myself, the program does not start.
But I have changed the settings to build:
# define VECT_TAB_OFFSET 0x10000 in system_stmf4xx.s
FLASH (rx): ORIGIN = 0x08010000, LENGTH = 1024K in stm32f4_flash.ld

The compilation is done well with the offset. I do not have too many ideas where to look.
I'm on atollic 3.3.

Thank you for your time.

Outcomes